Other Parts Discussed in Thread: LMH0376, LMH0356
We have a fibre-optic receiver board receiving HD-SDI (SMPTE292) video data. The output of the fibre transceiver is fed directly into channel 0 of the '356. The output goes to a buffer amplifier then to a BNC connector. The eye diagram I get from the output is poor (jitter is ~250ps after 5ns). If I feed the output to the SD3GDA eval board the LMH0376 chip cleans the signal up a treat.
What could possibly be wrong with the '356? We thought originally that the bypass pin might have been inadvertently pulled high, but no. The LOCK DETECT is high. SD/HD_n is low. The 27MHz crystal appears to be working OK. It's as if it were in BYPASS mode - but it isn't.
Originally our board was fitted with loop filter capacitor 560p (don't know why). We changed to the recommended 56n - no observable improvement.
Any thoughts?
Regards,
Richard