This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913Q/914Q GPI/GPO Control Clock



Hi, Let me questions about DS90UB913Q/DS90UB914Q.

1) If each clock has not been entered in the DS90UB913Q of CLKIN (18pin) and PCLK (3pin),  

    Signal input to the GPIO0 (28pin) and GPIO1 (27pin) of DS90UB914Q is,  

    Do you are output to the DS90UB913Q GP00 (15pin) and GP01 (16pin)?

2) If there is no PCLK, or GPIO will work with the device's internal clock?

Best regards