Other Parts Discussed in Thread: ADS7040
Hey All,
Is there away to transfer the data between two i2C or SPI devices without using a micro controller? For example, I have a nRF2401 SPI based 2.4 GHz transmitter and a SPI temperature sensor. How can I just make the temperature sensor constantly dump data to the SPI 2.4 transmitter with out a MCU? Is there a programmable device that can generate the clock, with the correct timing?