This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75451BDR temperature performance



We operate the SN75451BDR at ambient temperatures between +20C and +60C, with short-term operation as low as -20C (system start-up). 

The SN75451BDR is rated for use between 0 and +70C.

It appears that wider temperature versions are not available in the SOIC package and we are trying to avoid a board revision.

My question is related to use of the SN75451BDR device at -20C.  Some details on our application follow:

    The board containing this device is conformally coated.

    Worst-case power dissipation (both channels combined) < 100mW; well below the max rating of 464mW at +70C.

    All inputs are driven by similar logic devices (all 5V), and output high voltage is also 5V.

    Maximum switching rate is very low (<1kHz).

What parameters or functionality should we be concerned about for -20C operation?

Regards,

John