Other Parts Discussed in Thread: DS125DF1610
Our hardware design has a DS125DF1610 sitting between a switch ASIC and the SFP+ cages (plus a 2nd design that uses 2xQSFP+ instead of 8xSFP+).
[98DX4251] --- |connector| --- [1610] --- [SFP+]
Please help with the following questions:
1) Initialization of CDR chip relative to channel inputs. Can we configure all of the 1610 channels before bringing up other components in the data-path or do we need to configure it as we enable the serdes output from the switch ASIC. Do we need to actively configure the line-side based on the SFP+ MOD_ABS or RX_LOS (note RX_LOS won't help when using direct attach cables).
2) Reaction to external events. If the switch ASIC port is disabled/enabled via user command should we re-initialize the associated channel(s). Similarly if the SFP+ module is removed/replaced should we re-initialize (presumably we should if we're changing from Fibre to DAC and need to apply different parameters).
3) Have you got any example configurations for the 1610 with SR/LR Fibre
SFP+ modules?
Thank you