Other Parts Discussed in Thread: ISO7220C, ISO7320C, ISO7821, ISO7841, ISO7842
Hello,
I use the ISO7220C digital isolator to separate my micro-controller part (F28335) from my power part (IGBT inverter). So isolators are used to propagate the PWM IGBT commands from the DSP to the inverter.
My typical DC voltage is around 600V (three-phased 400Vac / 50Hz network, rectified throught a diode rectifier, then filtered).
I an currently experiencing some EMI effects when working at 600V : inverter's IGBT drivers seem to be disturbed and commute in an erratic way, inducing the drivers in error state.
When I work at 320V (monophased voltage rectified), I have no problem.
Previously I used no isolators for PWM signals, and got similar problems but at much lower voltages (at ~100V the problem begun) ; thats why I added the isolator : that solved the problem until 320V, but now that appear again at 600V...and I have no DC supply to check the behavior with DC voltage in the interval 320V/600V.
Reading carefuly at the isolator datasheet, I found the Maximum Working Insulating Voltage to be 560Vpeak, so just a little bit under 600V.
Is it possible that this isolator is not the correct one to work under 600Vdc ?
Shall I change for an isolator with re-inforced isolation (like the ISO7521CDW) ?
Thank you,
Best regards,
Julien