This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI86 Any limitations on HPW/HBPR, also ASSR support

Other Parts Discussed in Thread: SN65DSI86, TEST2

Hiya,

I'm looking at SN65DSI86 to replace a similar-function DSI>eDP bridge from Toshiba and I have some questions.

Toshiba part requires that minimum HPW+HBPR must be >= 48pixels for 4channel eDP transmission. The datasheet for SN65DIS86 doesn't mention anything like that. Is there such limitation, or can I use ex. HPW = 5 and HBPR = 7 or so. HPW = hsync pulse width, HBPR = hsync back porch.

Regarding ASSR, there's following information on the internet: "for Non ASSR panel, need a HW stripping please contact TI to get more information". Any.. more information on that?

Also, I plan to access this part only via the DSI0 (DSI Channel A) configuration registers (I2C will be not-connected). Is there any special settings I need to do prior to this from the DSI master, such as setting LPTIME etc.