Other Parts Discussed in Thread: TUSB9261
Hi Everyone,
Now our customer has calculated the discrete capacitor values by referring SLLA122, then they need to know the capacitance of XI and XO. I know that XI input capacitance is stated in section 7.8 in datasheet. Then;
- Does is include any parasitic capacitance? I think 0.414pF (typ) is quite lower than 2 pF – 5 pF stated in SLLA122.
- Is the XO input capacitance the same with XI input capacitance?
What I'd like to know is the Cdevice to calculate CLoad at TUSB9261.
Best Regards,
Sonoki / Japan Disty