This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB940 master mode



Dear Sir

I would like to use DS90UB929 and DS90UB940 for HDMI to MIPI Panel 

I have some question

1. DS90UB940 can't be a master mode to read SPI Flash or EEPROM register automaticly ,Is it right? ( 940's SPI or I2C will pass the signal from host side or device side)

2.If I want to use one pin of DS90UB940 to controller "MIPI Mux 2:1 switch" channel selection when HDMI cable insert in DS90UB929 (PS. DS90UB940 detect some of signal deliver from DS90UB929)

How could I do this function??

Thanks