This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP139 swap innput and output's poisitive and negative



if customer swapped DP139 input(DP data) and output(DHMI)'s positive and neagtive pin, is it ok to work chip?...As I know, HDMI is O.K, how about DP input?....

  • DP139 input data is agnostic to polarity as well as orientation.  Polarity of the differential signals is not critical to the operation of the device.  It is however critical to the operation of the  DP++ to HDMI interface.  If a polarity change is done on the input, the output will also need to be inverted.  True polarity must be maintained from the DP++ source to the HDMI connector interface. In_D1, In_D2, In_D3, In_D4 can also be “re-arranged” to allow for a better layout.  Again, the DP++ source and the HDMI connector must match signal mapping

    Typical DP++ mapping is the following:

    DP139:In_D4 to Out_D4 is TMDS CLK

    DP139:In_D3 to Out_D3 is TMDS D0

    DP139:In_D2 to Out_D2 is TMDS D1

    DP139:In_D1 to Out_D1 is TMDSD2

    Ken