Other Parts Discussed in Thread: DS125BR820, DS100DF410, DS100KR800, DS110DF410
Hi,
I design SFP+ host to QSFP host media converter/repeater. Simply, the board where is four SFP+ cages on one side and one QSFP cage on other side, each SFP+ host connected to one channel in QSFP host (crossover RX -> TX and vice versa). Hosts must meet the condition SFF-8431 (or SFF-8436) hi-speed interface specification.
Primary, in SFP+ cages will be various optical modules and in QSFP cage will be copper twinax cable (up to 5m), but solution must meet the requirements for combination of copper cable or optical modules in each host. I expetimentaly try only passive solution and it (experimentaly) works with DELL optical modules in SFP+ hosts and max 0,5m copper cable in QSFP host.
I am thinking about simply design for solution with active components, place between SFP+ hosts and one QSFP host channels some repeaters (4+4 channels together). So, my question is, what is better to use as these repeaters, redrivers or retimers? I understand the difference, how both of them theoretically works, but I need advice for application usage. I am looking for TI products, e.g. DS125BR820 from redrivers or DS100DF410 family from retimers.
Thanks!