Other Parts Discussed in Thread: TLK2711-SP
Hello,
I've been reading the following application briefs with respect to jitter analysis:
SLLA149 - Refclk Jitter Analysis for the TLK2521
SLLA071 - Understanding Jitter and the Bit Error for the TLK2500
I'll be using the TLK2711-SP for an application and was wondering if this information is comparable to this device or is there similar data available that was collected specifically for this device?
1) Can I assume the PLL bandwidth of the TLK2711 is also around 10MHz? (Ref. SLLA149 pp 2-3)
2) By similarity, would jitter transfer within the PLL bandwidth be on the order of 1dB to 2dB? (Ref. SLLA149 p4)
3) Is there an EVM available for the TLK2711-SP?
4) Is there any data showing the relationship between votlage ripple measured at the VDDA pins and jitter on the serial output? How much ripple can be tolerated at the VDDA pins?
Thanks,
--Rick