Other Parts Discussed in Thread: ALP
Hi,
I have MTA customer who is starting to evaluate the device using EVB and ALP and would like to understand the following points:
1-In order to start the device, do you need to connect to PC and set registers or the device can be started with the default configuration , if it is ok for the application?
2-Is there a way to save last configuration used or do you need to rewrite everything at power on?The ALP program refers to an EEPROM daugher board, when changing the profile, but is it something to be supplied apart?
3-In order to change the registers contents, do you have to write one by one, or you can run a script that automatically changes all you need?How can you do it?
4-Is there a way to set a custom pattern(not monochrome, for centering or fickering control purposes) and there is a way to run automatically in sequence a set of custom patterns?I see only possibility for the std. patterns.
Thanks
Umberto