Other Parts Discussed in Thread: SN65HVD3082E, SN65HVD1780
I am looking for help on deciding the best RS-485 transceiver chip for my application. I need a chip with the following qualifications:
- 5 volt power
- Fails safe Idle, open, short
- 8PDIP
- Half duplex
- ESD protection
- Low EMI
I have already looked around and like the SN65HVD3082E and the SN65HVD1780.
I chose these because of there longer rise/fall time which I understand reduces EMI. For the application we only need to run 19.2kbps at a MAX distance of 100 feet.
Me being new to this field of communications can anyone help me decide which transceiver would be best for my application or if you have a better chip in mind I would love to here about it.
Thanks for the help!