Other Parts Discussed in Thread: DP83848K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DP83848K
Hi,
By another thread, I understood how to configure the DP83848 registers to generate test patterns for 10Base-T.
Could you tell me about 100base?
In the case of 100base-T, I think that the compliance test is possible with IDLE pattern. So,It is only set to 100base the DP83848.
Is theis correct?
Best Regards,
Taka
Hello Taka-san,
You are correct, configure the device for 100Base-T operation.(write the BMCR, register 0, to a value of 2100h.
This will configure the device to 100Base-T, Full Duplex.
Are you using a commerical compliance test suite? If so, would it be possible for you to share thisinformation with me?
Thanks,
John
Hi John-san,
Thank you for you reply. I understood it.
John Hamilton1 said:Are you using a commerical compliance test suite? If so, would it be possible for you to share thisinformation with me?
I will confirm the type of compliance test to my customer.
If yes, what kind of information do you want?
Best Regards,
Taka
Hi Taka-san,
In my lab I use the Tektronix TDSET3 Etherrnet Compliance test Suite.
I know that there are other compliance suites available from other vendors.
I would like find out the types of tests suites being used so that I could build
up my knowledge base with the different test suites.
Thanks,
John