Other Parts Discussed in Thread: PCA9306
Hi,
There are questions in IBIS modeling of PCA9306.
setup is as below.
4.7kohm pull up and transmission line are used because there is no test load guidance.
IBIS model is used per each VDD because [Model Selector] is not needed in case of series switch model,
Phenomenon
1. there is very little difference between max/typ/min
2. typ case and max case is almost same in case of 5V VDD
Are these phenomenon correct results?