Other Parts Discussed in Thread: TUSB7320
Hello,
I am trying to understand the USB receiver phy equalization settings of the TUSB7320
PORT1_EQ_OV
PORT1_EQ_FUNC
PORT1_EQ_INIT
On our controller
- Equalizer Control Register E8h
- Custom PHY Transmit/Receive Control Register ECh
are both 0000 0000h.
Does it mean that no equalization is done or is it done?
According to the datasheet Port 1 Equalization Override (PORT1_EQ_OV) = 0 means that the default equalization settings are not overridden. But what are the default equalization settings?
I was astonished that it is possible to switch of receiver equalization.
I had thought the receiver equalization using the TSEQ sequence was part of the USB 3.0 standard. Is it really possible to deactivate it on the TUSB7320?
Thanks,
Christian