This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH1218 VDD decoupling capacitor

Other Parts Discussed in Thread: LMH1218EVM

Hi, TI I'd like to confirm the decoupling capacitor value. The datasheet(SNLS474A –FEBRUARY 2015–REVISED MARCH 2015) recommended 0.01uF X 2 for VDD, but the LMH1218EVM(snlu173a) using 0.1uF X 2 . Which do you recommend 0.01uF or 01uF for VDD decoupling capacitor ?
  • Kobayashi-San,

    You can use 0.1 or 0.01uF Capacitor. This attenuates the high frequency noise. Based on PCB noise, you could decide whether you need to use 0.1 or 0.01uF Capacitor but either one should work. Please make sure you also use a high Capacitor value, 1 or 10uF Capacitor in parallel with 0.1 or 0.01 uF as well to attenuate the higher frequency noise.

    Regards,,nasser