This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK2711 at reduced data rates

Dear all,

Basically, we wanted to use TLK1501 and TLK2501 to transmit/receive data at rates of 0,6Gbps and 1,2Gbps.

But they are not compatible with our application due to their specific K-code usage (we need a full K-code control), therefore it seems that only TLK2711 supports K-code control.

1) In this way, I'd like to know if the TLK2711A can work at a reduced speed of 0,6Gbps to 1,2Gbps?

2) There is may be a way to use half of the bandwidth?

3) If not, is there any way to adapt TLK2501/1501 to control K-codes as TLK2711 does?

Thanks in advance,

François.