This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH927Q-Q1 Serializer with the DS90UH926Q-Q1

Hi i have an TFT LCD which is of 8-Bit (R0-R7,G0-G7 and B0-B7), i am using the DS90UH927Q-Q1

Can i use DS90UH926Q-Q1 deserializer to run my TFT LCD or do i need use DS90UH928Q-Q1 along with the Driver IC which convertes FPD link III to RGB lines?

if need to use an driver means please provide us the driver part number?

Please let me know at the earliest.

Thanks & regards

Yogesh.

Ph no. +919964434397