Other Parts Discussed in Thread: TRS3253E, TRS3232, MAX3223, MAX202
Hi,
We have an application where a 1.8V to 3.3V board talks to PC via RS-232. The signal is a subset of the DB9 which consists of TXD,RXD,RTS,CTS.
As the voltage needs to be translated to 15V level to communicate with PC, and down to 1.8-3.3V level when back, does any transceiver integrates internal DC converter/charge pump to do this?
Please recommend three to four modules for us, thanks!
And please also point out if any of them has EVM available. It is preferably that the EVM has input and output headers (allow inserting wires/connectors from other boards) for readily serving as a voltage bridge between low-voltage board and PC.
Matt