Other Parts Discussed in Thread: TUSB9261
Hi all,
We have TUSB9261 in our custom board to be used as SATA to USB bridge. After power up the device is detected as "TUSB926x Boot Loader device" in TUSB926xFlash Burner Programmer Software (On Windows 7 32-bit OS).
I have downloaded the firmware from ti website (TUSB926x Default Firmware, U1/U2 Disabled (Rev. L) (ZIP 446 KB )). But the firmware file is getting downloaded without any extension. If I select this and click on Program, It is giving error message as "The selected file must have a "*.bin" or "*.hex" file extension. I have renamed the file with ".bin" extension, but when I click on program it gives error as "The firmware file must be under 64513 bytes". I have tried renaming the file as ".hex" file also, but it shows "The selected .hex file is not valid".
Can you suggest me what might be the reason for this problem and how can I resolve this.
regards
Lingaraju