Other Parts Discussed in Thread: PCA9306
Hi,
In PCA9306 IBIS model,
There is C_comp parameter and there are min, typ and max.
And there are current value per each C_comp.
Question is
Does min value mean minimum of C_comp not current?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: PCA9306
Hi,
In PCA9306 IBIS model,
There is C_comp parameter and there are min, typ and max.
And there are current value per each C_comp.
Question is
Does min value mean minimum of C_comp not current?
Thanks.
Hello Adam,
Typically, the Min, Typ, and max values define the window of variance you will see across a large sample of devices.
You are correct that min value means the minimum of C_comp, not the current value.
Hi Jonathan,
Could you provide a relationship between C_comp and series current to the customer?
Customer couldn't understand clearly, why lower C_comp shown higher current value than higher C_comp.
Thank you.
Best Regards,
Jade
Hi Jonathan,
Please refer PCA9306 IBIS model script.
|******************************************************************************
[Model] PCA9306_IO_50A_S
Model_type Series_switch
|
|
| variable typ min max
C_comp 0 0 0
[Temperature Range] 40 100 -40
| Ambient temperature 25 85 -40
[Voltage range] 5 5 5
|
|******************************************************************************
[On]
[Series Mosfet]
| PCA9306_IO_50A_S
Vds = .5
|
| Voltage I(typ) I(min) I(max)
|
0.0000e+00 3.2508e-11 2.8399e-09 2.6694e-11
7.1000e-01 9.0123e-11 2.8143e-09 4.3039e-06
7.8000e-01 4.9796e-10 2.8143e-09 4.8010e-05
7.9500e-01 7.4239e-10 2.8144e-09 1.1077e-04
8.1500e-01 1.2733e-09 2.8148e-09 3.3879e-04
8.3500e-01 2.1946e-09 2.8154e-09 7.2247e-04
8.5500e-01 3.7933e-09 2.8164e-09 1.2525e-03
8.7500e-01 6.5673e-09 2.8181e-09 1.9201e-03
This model C_comp is "0" but still shown current min value is higher than max value.
Not only this model but also several C_comp "0" model show similar results.
You can see sometimes min value is higher than max value and sometimes min value is lower than max value.
They think min value is always lower than max value when C_comp is 0 condition.
Could you check their question?
Thank you.
Best Regards,
Jade