Other Parts Discussed in Thread: LMH1983, LMH1981
I have the LMH1981 chip connected to the LMH1983 chip and PLL4 is connected to an FPGA configured for 24.576MHz output. The LMH1983 is in default mode, which should put the chip in Genlock mode and with LOR the part should go into holdover mode. When I connect a blackburst source, everything works great. When I disconnect the blackburst source the LMH1983 does not seem to go into holdover mode. It seems like the control voltage to the oscillator is at .4V so it is obviously not holding over the 1.68V I read when the blackburst source is connected. Any ideas?
My only thought is to change the default behavior to go freerun with LOR and setup the voltage control to 1.65V but that really isn't holdover.
Thanks.