Other Parts Discussed in Thread: DP83848I
Dear Experts,
I have a quick question related to the power-up to link-up time of our DP83848I:
"As far as we understood from the datasheet and the forum threads, it takes 167ms from power-on until it achieves functional status. This was mostly to guarantee the stability of the 25Mhz clock source.
What we would like to know is the time it takes from power-on until the IC links up?
To be clear, on the other side we have a card that is ready for communication. Assuming that card also has DP83848I and is ready for cummunication, what would be the link up time of the DP83848I from power-up until it links up with the other DP838348I on the other card waiting for communication? "
This is the last point needing to be answered to be able to DWIN our device in this project.
Thanks,
Murat Ilhan.
TI-Turkey.