hello,
I'm in the process of evaluating LVDS (and MLVDS) communication between 2 or more boxes. I'll be using the SN55LVDS31 drivers and SN55LVDS32 receivers. I have several configurations including direct connection and AC coupling with capacitors or transformers.
Single-point grounding (SPG) will be implemented on the boxes and the boxes are isolated from each other.
One question that I'm trying to answer is : whether I use AC coupling or not, will common-mode noise transmit from one box to another?
I bread boarded a setup where the driver and receiver are powered from different power supplies and they are offset from each other. I used AC coupling with capacitors and the transmission was good for any offset between the power supplies. My colleague is telling me that this is not a test for common-mode noise.
I'm not knowledgeable about common-mode noise. Any suggestions would be appreciated.