Other Parts Discussed in Thread: LMH0302, LMH0344
Hi,
I have an application where I have a LMH0302 which needs to drive two SMPTE outputs. There is no guarantee that there will be a smpte monitor connected to both SDO and SDO_BAR at the same time. In some cases, SDO will be connected, in other cases SDO_bar may be the only output connected and finally in some cases they will both be used simultaneously. Will that be a problem?
Also can I assume that if both monitors are being used then the image will be identical on both even though one is generated from the compliment output?
Thanks,
Mitch