Other Parts Discussed in Thread: DS90C383, DS90CR287
Hello
Earlier, we used DS90S383MTD no problems.
Subsequently, we replaced it of DS90SR287, circuit and elements unchanged. In most cases, the image on the LCD module is displayed without any problems.
But sometimes, when power is applied, the colors displayed on LSD distorted, for example, black color is painted in blue. Eliminate distortion can turn off the power and then turning on the power.
Frequence CLK 65 MHz frequency.
LVDS cable length of 0.3 meters
Do you think, what could be the problem?
What function 17 pin in DS90SR287? In DS90S383MTD 'it was R_FB. Are there special requirements to it at power?
Thanks