hello,
My colleague is claiming that it is better to use 2 single-ended probes rather than using a differential probe when generating LVDS eye diagrams on an oscilloscope. When using 2 single-ended probes, use the math function to subtract one signal from the other and it will give the "true" difference between the +/- pair at the receiver. My colleague claims that differential probes are meant for probing signals with respect to a floating ground and is not meant for obtaining the difference between 2 signals.
Can someone comment on this? is there any truth to what he is saying?