Other Parts Discussed in Thread: DP83640
Hello,
We have a DP83640 Precision PHYTER implemented on a card and we are having issues with variable link times. The link times seem to vary from card to card and over time and appears to be bimodal in that the link times are either about 248 ms or about 320 ms. So far no other link times have been observed. We are strapped for 100BASE-TX, Full-Duplex, Auto-negotiate disabled. This behavior is causing system level timing issues. What connections to the PHY or other conditions could cause this type of behavior? Could one of these link times be considered nominal and, if so, which one? We have seen cases where a card will power up with the faster link time and then slow down on subsequent power cycles, but we have also seen the reverse. Anyone have any ideas on what might be going on here?
Many thanks,
Damon Pritchett