This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to connect a 10 bits data camera device with DS90UB913?

Dear All:

I want to connect a 10 bit camera to 913, i am not sure about

camera data 9:0=>913 D9:D0 or camera data 9:0 =>913 D11:D2???

If use a 8 bit YUV output camera,how can i build the connection

camera YUV data7:0=> 913 D7:D0 or camera data 7:0=>913 D11:D4???

The left 913 data pins should tie to H or L or just left open?