Other Parts Discussed in Thread: DS90UB926Q-Q1
Hello,
I'm trying to debug an issue on a DS90UB926Q-Q1 where the expected 7'b address is 0x39 and the actual address is 0x3A.
Most of the hardware that we built works as expected but some of them are defaulting to 0x3A instead of 0x39. I'm just wondering where I should look.
Like the datasheet shows on page 32 we have a 137k ohm resistor for R1 and a 191k ohm resistor for R2. Ideal VR2 measure at 1.902V and VDD33 measure at 3.235V for an ideal ration of ... 0.588.
Where should I look, when does this IDx pin 56 get read? Rising edge of PDB?
Andrew