Hello,
We are currently using the TUSB1210. When we use it in UART mode, which pin is the TX (output) and RX (input) to the chip? From figure 5.1 in the datasheet, our assumption is DP is the input and DM is the output. However, we don't see that stated anywhere, and want to confirm. DM is connected to pin 2 on the USB connector, which is an input (I believe), DP to pin 3 (output), so, we want to verify what to expect in UART mode.
Thank you