This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848 Connection to single Differential Pair (10Base2)

Looking at the DP83848 spec I see that it supports full and half duplex modes. The chip can also detect collisions. Thus I was interested in trying to use this chip (or similar chip) to implement a half duplex interface at 10Mb. Can I connect the chip up to support a singe differential pair or coax wire interface between to boards?  I have been reading about how 10Base2 and 10Base5 works but have not seen a recent way to implement this.

Chuck

  • Hi Chuck,

    DP83848 does support half duplex communications for 10BASE-T networks utilizing shared-medium hubs where multiple devices are in the same collision domain. The TX and RX pairs are still 2 separate differential pairs (4 conductors) and a 10BASE2 configuration would require one of these pairs to alternate between TX and RX duties. DP83848 doesn't support this operation.

    If you are interested in using Ethernet across a single diff pair, please send me a friend request so we can discuss it further.

    Best Regards,