Other Parts Discussed in Thread: DS16F95
I have a space component requirement (surface mount / -20C to +100C) for a RS-485/422 transceiver that is capable of a 20Mbs serial data rate but will actually be used at 10Mbs (de-rating).
The DS95F174MJ-QMLV and DS95F175MJ-QMLV datasheets specifically state that they can support up to 15Mbps where the F95 does not specify this.
The bus is <40' long.
I was told by ti support that the DS16F95 uses the same process and design elements as the 174 and 175.
Can the F95 support 15Mbs over the above temperature range?
This may be an acceptable tradeoff from 20Mbs.
Thanks.