This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Output Resistance Value not matching the Table - TPL0501-100



I try to vary the output. resistance value Rwh , Rwl not matching the table value.

is any calculation required to get the output compare to the table? 

  • Hello Arun,

    Thanks for the question.

    This is actually a mistake in this datasheet that we are currently in the process of correcting.

    RHW and RWL are backwards, so when at step 0, RWL is 0 ohms, when at step 255, RWH is at almost 0 ohms, as such, the ratio is also backwards.