Other Parts Discussed in Thread: SN65LVDS93A-Q1
I have many questions about application of the SN65LVDS93A-Q1. Thank you in advance for answering them.
(1) In the schematic example in the SN65LVDS93A-Q1 datasheet, the data inputs all have external 4.7k ohm pullup resistors. Is 4.7k ohm pullup on data inputs recommended for application?
(2) For our data inputs that we are tying only what value resistors should we use to tie them to the rail?
(3) Can we tie GND pins directly to the ground plane, or do we need a resistor or something inbetween GND pin and ground?
(4) Figures 15, 16, and 17 show PLLVCC and LVDSVCC tied together, while figure 13 shows PLLVCC, LVDSVCC, and VCC tied together. Is it recommended to tie PLLVCC, LVDSVCC, and VCC together, and use the same decoupling caps? If not, is it recommended to tie PLVCC and LVDSVCC together, and use the same decoupling caps?
(6) If our IOVCC is going to be 3.3V, can we tie VCC, PLLVCC, LVDSVCC, and IOVCC all together, and use the same decoupling caps?
(5) What is the purpose of having a .1 uF and .01 uF caps in parallel for power pins? Why not just one .11 uF cap?
(6) If our IOVCC is going to be 3.3V, can we tie VCC, PLLVCC, LVDSVCC, and IOVCC all together?
(7) The DS90UR905Q needs series decoupling caps for its output LVDS lines. Do the LVDS output lines for the SN65LVDS93A-Q1 need series decoupling caps?
(8) Should the input pixel clock have a 50% duty cycle? we will want the output pixal clock to have 4/7 duty cycle. Will the serializer make the change from 50% to 4/7 duty cycle by itself?
Thanks again