Other Parts Discussed in Thread: DS92LV2421, DS92LV2422, DS90UB925Q-Q1
We would like to use the DS92LV2421 to create a serial DVI stream to send over fiber.
The datasheet states a 75MHz clock rate maximum.
We need about 77MHz.
The Spread Spectrum spec at 75MHz is 35kHz with a +-2% fdev.
Is the +-2% fdev considered to be 2% of 75MHz?
If so then +2% of 75MHz is 76.5MHz.
I do not intend to use spread spectrum, thus can I run my clock up to 76.5MHz?
I really want 77MHz, just 500kHz more.
Can you comment on the performance of the DS92LV2421 with a 77MHz clock?
Thank you.