Other Parts Discussed in Thread: TLK105L, TLK105
Hi,
My customer are having trouble with TLK105L LED_LINK.
The LED_LINK pin is pullup with 2.2k, so that it is low active.
When LINK is ok, the LED will LINK. But when the transmitter or receiver is active, LED doesn't blink but it will link.
They are setting the register as follows:
Case1. <MLED is not routed to LED_LINK(17pin)>
(1)LED Control Register (LEDCR), address 0x0018, value = 0x0600
(2)PHY Control Register (PHYCR), address 0x0019, value = 0x8000
(3)Multi LED Control register (MLEDCR), address 0x0025, value = 0x0040
Case2.<MLED is routed to LED_LINK(17pin)>
(1)LED Control Register (LEDCR), address 0x0018, value = 0x0600
(2)PHY Control Register (PHYCR), address 0x0019, value = 0x8000
(3)Multi LED Control register (MLEDCR), address 0x0025, value = 0x0043
In either case, LED doesn't blink but it will link when the transmitter or receiver is active.
Are there any register need to be configured?
And are there any reason why LED doesn't blink?
best regards,
g.f.