Other Parts Discussed in Thread: TPS62086, TSU6721
Hi, I have tried several cheap Chinese power banks and they seem to power the TSU6721YFPR just fine. I have a fancy one however, and after about 30 seconds the power bank powers off. Is this a negotiation problem or something I did in managing pins?
In order to utilize the BGA TSU6721 (and it is necessary to utilize the TSU6721 to get OTG + BCD1.2 and have the USB data lines lay out on a single layer), I shorted the MCPC output lines to near by necessary lines. SCL connects to C3, SDA connects to MIC, S_R, and S_L, IDBP connects to RxD. OUT actually does drive the a SMPS (TPS62086) producing 3.3V VDD. Is there any reason the pin shorting could trigger a properly designed power bank to shutdown? Could the TSU6721 be throwing an error that shutsdown 30s in or negotiate a power down for some reason?
Thanks,
Chris Hamilton