Other Parts Discussed in Thread: TUSB8041
Customer produce : U3H41S4310S,
It is USB 3.0 to four SATA III Bridges Board with Read-only (Write Protect) or Read/Write Function
http://www.ioi.com.tw/products/proddetail.aspx?CatID=101&ProdID=1010145&HostID=2035
USB3.0 HUB is TI USB8041 / SATA III Bridges is ASM1153E
OS: Window 7 SP1 64bit
Setting :
-
Upstream port: USB3.0 Cable connector U3H41S4310S and Host USB3.0(intel hsot)
-
Downstream port: : We use SATA7pin Cable connector U3H41S4310S and SATA HDD
-
HDD use External Power
We power on the first HDD Power than Power on ASM1153E
All function test will be pass.
BTW:
Issue : We power on the first ASM1153E than Power on HDD power ,
If HDD did not have Partition , We open the Computer management , The system will be Stop.
If HDD have Partition , we can read / write / format HDD , but we can not delete Hdd Partition in Computer management ,
We have test in TI TUSB8041/TUSB8040EVM have same issue , but we change VIA USB3.0 HUB, this issue will be fixed.