Other Parts Discussed in Thread: TUSB8041, TPS2561, TPS2560
Hello, I have found what I think is a contradiction on the datasheet for the TUSB8041. On page 33 of the datasheet, there is a statement about the reference design shown in the datasheet that says: "The PWRCTL_POL is pulled down which will result in active high power enable (PWRCTL1, PWRCTL2, PWRCTL3, and PWRCTL4) for a USB VBUS power switch." However, the pin description on page 7 indicates that a "1 = PWRCTL polarity is active high". Is this an error of some sort?
I also have a question regarding the use of this part. I would like to set this up to be a HUB that does not need to be configured, so I think that I need to set it up for I2C mode. That's easy enough to do, but I am wondering if I have to have a memory device attached or if I can get by without a memory device on the I2C bus. Can you help with this?
Regards,
Ben