Other Parts Discussed in Thread: TLK3131
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TLK3131
Hi Luis Omar Morán Serna
1. There isn't protocol in particular.
2. My customer requirements are to realize the following transformation.
8bits pair * 96 <-> 8b/10b <-> Serialize/De-serialize <-> 96 channel
(Reference Clock =160MHz, SerDes Data Rate = 1.6Gbps)
Is it possible to realize by TLK3131 at 96pcs or TLK3134 at 24pcs?
Can these device(TLK313x) be used as General Purpose SerDes like the above?
If it's impossible, are there other solutions which can be proposed?
Best Regards,
itabi
Hi Itabi,
In EBI mode is not fixed, just for XAUI mode but I would like to double-check with the designers.
Best Regards!
Luis Omar Morán Serna
High Speed Interface
SWAT Team