Hello,
On any given US or DS port of the TUSB8040A hub, is the LFPS detection circuit first filtered by a low-pass-filter? I.e. Can a signal that is higher than allowable LFPS frequency (higher than 50MHz) trigger a U3 wake-up? Other than the amplitude, what metrics does the TUSB8040A enforce on the received LFPS signal to determine if it is valid LFPS or invalid LFPS, with regards to a U3 wake-up?
Thanks,
KT