Other Parts Discussed in Thread: TUSB320, TPS2511, TPS2561A, TPS2543, TUSB320EVM
Hello. I am interested in using the TUSB320 from TI and configuring as a UFP. The chip would be in a mobile battery pack, for example, and would communicate to whatever usb c host there is, through the 24-pin USB C connector. I really don't care about the data lines. I just want to use the power from the host (and also use some of the spare data lines to provide MORE power for faster charging, and would use a 1:2 switch to switch the lines between two different circuits).
I know the TUSB320 would present a pull down resistance on the CC pins, since it is acting as a UFP.
I have looked at a schematic in the TUSB320 datasheet (figure 14) where the TUSB320 is in UFP in I 2C Mode Schematic. I would want to use it in this way, basically, but the schematic does not show what is done with the USB 2.0 and superspeed diff pair data lines. I want to know if there is a chip like the TPS2511, but for the data lines on a USB C connector. That is, is there some sort of chip that I can put down on my board and connect the data lines to so that i still get power from the host but have all other data lines (besides the CC pins of course. Maybe i need those to work between the host and my TUSB320)?
My concern is that if I just leave all of the data lines unconnected/open on my board, then the host will give freak out and decide not to provide any power at all. Is there any reason to believe that the host would quit supplying power all together if the all of the data lines (except CC pins!) are just left open? Because that's probably the simplest solution in my mind. Or, I can just short them together. I'd do that if I know that's ok. That's easy to. I want my battery pack to work universally, with any kind of usb c host.
Also, I am looking for a schematic for the TUSB320 Evaluation modul (EVM). I can't find a schematic on the product's TI web page. But, I wonder if the answer lies there. That is, if the designers of that board already know about this, they designed the module to provide power even though all of the data lines (besides CC pins) were just shorted together or left open.
Looking forward to a response! Sometimes I don't have luck with forums..
Matt