Other Parts Discussed in Thread: LMH0340
I am looking at an application where I need to create a SDI output from a LVDS/HDMI Interface. I am looking for SMTPE 424M. I believe I can get SDI rates up to 2.97 GBPS which will allow 1920 x 1080 @ 60 fps. The datasheet shows a 5 bit LVDS (5 diff pairs) and the LVDS CLK which is then 8b/10b encoded to a 5:1 Mux out to SDI and it talks about a FPGA attachment. So here are my questions:
1) This device will work only with 5 LVDS pairs running at what rates?
2) Is there anyway we can use different number of LVDS pairs and increase the data rates?
3) I plan to use a single SDI interface so can the SMB be disconnected with PUZs and the configuration goes to a default setting? Is the SMB Bus a must?
4) Do we need a FPGA to drive the LVDS signals? Can it not be driven by a Controller with correct LVDS data rate?
5) Do you have a similar device to go from HDMI to SDI?
Looking for a FAE who I can talk directly.