Other Parts Discussed in Thread: DS100BR210, DS100KR800
Hello,
I'm designing a PCB with the DS100BR210 in SMBUS master mode connected to EEPROM. I'm a bit puzzled with the statement on page 17 "The external EEPROM device must support 1 MHz operation" because evaluation board schematic suggests a 24C08 EEPROM. The standard 24C08 seem to be working up to 400 kHz but I couldn't find any working up to a 1 MHz. Also the 24C08 is an I2C version and not SMBus compatible.
So is the 24C08 a good choice or can someone recommend a different EEPROM?
I'm also wondering if the DS100BR210 as well as the DS100KR800 would work as a I2C slave? I was hoping that someone tried that already. I would appreciate some comments on that.
Thanks in advance!!