This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB7340 EVB circuit question?

Dear Sir

Form sllu146c.pdf P15, is PCI Express x1 Edge Connector "REFCLK+" connect to "PCIE_REFCLKN" and "REFCLK-" connect to "PCIE_REFCLKP"?

J4 USB3_TYPEA_CONNECTER, is "SSTXN" connect to "IND_DS_TXP4"  and "SSTXP" connect to "ND_DS_TXN4"?

J3 USB3_TYPEA_CONNECTER, is "SSTXN" connect to "IND_DS_TXP3"  and "SSTXP" connect to "ND_DS_TXN3"?

 SSRXN connect to "USB_SSRXP_DN3"? SSRXP connect to "USB_SSRXN_DN3"??

J2 USB3_TYPEA_CONNECTER, is "SSTXN" connect to "IND_DS_TXP2"  and "SSTXP" connect to "ND_DS_TXN2"?

J1 USB3_TYPEA_CONNECTER, is "SSTXN" connect to "IND_DS_TXP1"  and "SSTXP" connect to "ND_DS_TXN1"?

 SSRXN connect to "USB_SSRXP_DN1"? SSRXP connect to "USB_SSRXN_DN1"??

                                                                                               Best regards,

                                                                                                                Bogey