This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH940 Input mode



Hi TI, I'd like to confirm the FPD3 INPUT MODE(Add:0x34, bit 4:3) function. Is it possible to use the bit as a input selector ? My customer want to connect a DVD player(DS90UH925) to the primary input and want to connect a image sensor(back camera, DS90UB925) to the secondary input. And want to switch the inputs by using the FPD3 INPUT MODE function.