My application is for 2:1 mux with 1 input port-A is DP++ (DP 1.2a) and the other Port-B is HDMI 2.0 (6Gbps) and the output Port-C is HDMI 2.0.
1) Are both the AUX and DDC interface OD/OC (Open Drain/Open COllector)?
2) Should I configure the AUX_SEL at VDD/2, and route the DP++ (AUX) to DDC interface?
3) Should I configure the AUX_SEL to logic 'H' and set AUXC as DDC interface with +5V pull-up?
4) Lastly, does TI has a similar device such as HD3SS215 with EQ at 2 input ports and cable driver at the output.
Thanks in advance,
Duke